Android for Rooted Devices

The SDK 2.0 delivers cross-platform open source libraries & tools that allow users to develop on multiple Operating Systems & development environments. Intel has validated SDK2.0 on Windows and Linux platforms. Please check latest Release for the build versions. While Intel has not explicitly validated SDK2.0 on Android platforms, it is expected to work on Android as well. Please refer to the build instructions in the section below. Calibration and firmware update tools that would be used in production and manufacturing processes are not available on Android at this time. Please contact your RealSense representative for additional information.

Build RealSense™ SDK 2.0 for Android OS

This document describes how to build the RealSense™ SDK 2.0 including headless tools and examples for Android devices.

Disclaimer: There is a limitation in access to the camera from a native code due to Android USB permissions policy. Therefore, building RealSense SDK 2.0 for Android devices will run only on rooted devices.

Ingredients

Before jumping to the instructions section please ensure you have all the required accessories.

  1. Linux host machine with Ubuntu 16.04.
  2. Rooted Android target device that supports OTG feature.
  3. USB3 OTG cable.

Instructions of how to build SDK Headless Samples & Android Application

Last Updated: April 9, 2026

Top
Contact Sales
Server Region: Unknown | Hostname: ip-172-16-1-244 | Visitor Country: Unknown