Firmware Update Tool (rs-fw-update)

Goal

rs-fw-update tool is a console application for updating depth camera firmware.

Prerequisites

In order to update a depth camera firmware, a signed image file is required.
The latest D400/L500 camera firmwares are available here.
The firmware is packed into zip file and contains a file with “bin” extension with the following naming convension: “SignedImage_UVC<firmware_version>.bin”

📘 Note:

For Windows 10 users, the pre-built Intel.RealSense.FW.Update.exe executable file (.exe) is located at https://github.com/IntelRealSense/librealsense/releases/latest .

=> For other operating systems please install the SDK

❗️ Attention Lidar Camera L515 owners

Please use the device firmware update tool that comes with the librealsense SDK starting version 2.35.2.

Usage

After installing librealsense run rs-fw-update -l to launch the tool and print a list of connected devices.

An example for output for a D415 camera is:

HTML
connected devices:
1) Name: RealSense D415, serial number: 725112060411, ASIC serial number: 012345678901, firmware version: 05.11.01.100, USB type: 3.2

Then we will provide the serial number to identify the device together with the path to firmware file that we want to update rs-fw-update -s 725112060411 -f Signed_Image_UVC_5_11_6_250.bin.

An example for the expected output is:

HTML
search for device with serial number: 725112060411

update to FW: Signed_Image_UVC_5_11_6_250.bin

updating device:
Name: RealSense D415, serial number: 725112060411, ASIC serial number: 012345678901, firmware version: 05.11.01.100, USB type: 3.2

firmware update started

firmware update progress: 100[%]

firmware update done

device 725112060411 successfully updated to FW: 05.11.06.250

In case only one camera is connected you can simply run rs-fw-update -f Signed_Image_UVC_5_11_6_250.bin.

A camera/s might be in a recovery state, in such case listing the devices will output the following:

connected devices:
1) Name: RealSense D4xx Recovery, serial number: unknown, ASIC serial number: 012345678901, firmware version: unknown, USB type: unknown

In such case we can use the recovery flag and run rs-fw-update -r -f Signed_Image_UVC_5_11_6_250.bin

An example for the expected output is:

HTML
update to FW: Signed_Image_UVC_5_11_6_250.bin

recovering device:
Name: RealSense D4xx Recovery, serial number: unknown, ASIC serial number: 012345678901, firmware version: unknown, USB type: unknown

firmware update started

firmware update progress: 100[%]

firmware update done

recovery done

Command Line Parameters

FlagDescription
-sThe serial number of the device to be update, this is mandetory if more than one device is connected
-fPath of the firmware image file
-rRecover all connected devices which are in recovery mode
-lList all available devices and exits
-vDisplays version information and exits
-hDisplays usage information and exits
NoneList supported streaming modes

Last Updated: March 18, 2026

Top
Contact Sales
Server Region: Unknown | Hostname: ip-172-16-1-244 | Visitor Country: Unknown