Intel® RealSense™ Developer Projects & Code Samples
Explore a curated collection of Intel® RealSense™ developer projects and code samples. Find community-contributed examples for OpenCV, ROS, Unity, Raspberry Pi, and more.
- OpenCV DNN object detection with RealSense camera
- minimal_realsense2 - Streaming and Presets in C
- ANDREASJAKL.COM - Capturing a 3D Point Cloud with RealSense and Converting to a Mesh with MeshLab
- FluentRealSense - The First Steps to a Simpler RealSense
- RealSense ROS-bag parser - code sample for parsing ROS-bag files by @marcovs
- OpenCV threaded depth cleaner - RealSense depth-map cleaning and inpainting using OpenCV
- Sample of how to use the IMU of D435i as well as doing PCL rotations based on this
- realsense-ir-to-vaapi-h264 - hardware encode infrared stream to H.264 with Intel VAAPI
- realsense-depth-to-vaapi-hevc10 - hardware encode depth stream to 10 bit HEVC with Intel VAAPI
- EtherSense - Ethernet client and server for RealSense using python's Asyncore
- Unofficial OpenVino example + D400 - example of using OpenVino with RealSense and ROS for object detection
- keijiro/Rsvfx - An example that shows how to connect RealSense depth camera to Unity VFX Graph
- kougaku/RealSenseOSC - Client-Server project with Processing example for T265
- Vimeo Depth Viewer - A RealSense depth viewer using nanogui
- PINTO0309/MobileNet-SSD-RealSense - RaspberryPi3 or Ubuntu + Multi Neural Compute Stick(NCS/NCS2) + RealSense D435 + MobileNet-SSD(MobileNetSSD) + Background Multi-transparent(Simple multi-class segmentation) + FaceDetection + MultiGraph + MultiProcessing + MultiClustering
- realsenseOnCyber Realsense module Based on Apollo Cyber RT
- Raspberry Pi Handheld 3D Scanner by Frank Zhao
- Erwhi Hedgehog by Giovanni Bruno - Open-Source Hardware and Software design featuring RealSense, UP-Squared and Intel Movidius technologies
Updated about 1 month ago