TensorFlow
Introduction
TensorFlow is extremely popular open source platform for machine learning. This tutorial series will highlight different ways TensorFlow-based machine learning can be applied with RealSense Depth Cameras. We'll be using python as language of choice, but same concepts can be easily ported to other languages.
Example code can be found at the corresponding github page for this project at https://github.com/IntelRealSense/librealsense/tree/master/wrappers/tensorflow
Installation
We'll need the following components:
python 3.6- download page. Version 3.6 was chosen due to its compatibility with components belowpyrealsense2- on x86 Linux and Windows platforms can be installed by runningpip install pyrealsense2. For additional installation instructions please see official documentation. We'll be usingpyrealsense2to communicate with the camera and fetch frames from the device.numpy- We'll be using Numpy for image storage and manipulation. Install via pip install numpyopencv- We'll be using OpenCV for loading and saving images, basic image processing, and inference in some examples. OpenCV can be installed viapip install opencv-pythontensorflow- TensorFlow is the main focus of this set of tutorials. We'll be using TensorFlow version 2.3.0, or TensorFlow-GPU version 2.2.0. We'll also be using a version of Keras library bundled inside TensorFlow installation. Keras is offering set of declarative APIs simplifying network declaration and improving readability.
Note on GPU Support:In order to run TensorFlow with GPU acceleration on NVidia GPUs you need to install
tensorflow-gpupython package and compatible versions of CUDA and cuDNN libraries. List of compatible combinations
We assume you are already familiar with the basics of operating RealSense devices in python. Please see official documentation for more information and code samples.
Part 1 - Object Detection and Classification
RealSense Depth Camera can be used for object detection and classification with TensorFlow like any other video source. Example 1 is showing standard object detection using TensorFlow and data from the RGB sensor.
In order to run this example, you will need model file. Please download and extract one of the models from TensorFlow-Object-Detection-API page. We are using Faster-RCNN Inception v2 for this example, but other networks can be easily swapped-in. Extracted frozen_inference_graph.pb is expected to be in the working directory when running the script.
The code should be familiar with anyone who worked with TensorFlow before. We start by creating Graph object and loading it from file:
# Load the Tensorflow model into memory.
detection_graph = tf.Graph()
with detection_graph.as_default():
od_graph_def = tf.compat.v1.GraphDef()
with tf.compat.v1.gfile.GFile(PATH_TO_CKPT, 'rb') as fid:
serialized_graph = fid.read()
od_graph_def.ParseFromString(serialized_graph)
tf.compat.v1.import_graph_def(od_graph_def, name='')
sess = tf.compat.v1.Session(graph=detection_graph)Next, we will initialize the relevant input and output vectors needed in this sample:
# Input tensor is the image
image_tensor = detection_graph.get_tensor_by_name('image_tensor:0')
# Output tensors are the detection boxes, scores, and classes
# Each box represents a part of the image where a particular object was detected
detection_boxes = detection_graph.get_tensor_by_name('detection_boxes:0')
# Each score represents level of confidence for each of the objects.
# The score is shown on the result image, together with the class label.
detection_scores = detection_graph.get_tensor_by_name('detection_scores:0')
detection_classes = detection_graph.get_tensor_by_name('detection_classes:0')
# Number of objects detected
num_detections = detection_graph.get_tensor_by_name('num_detections:0')We'll start the camera by specifying the type of stream and its resolution:
pipeline = rs.pipeline()
config = rs.config()
config.enable_stream(rs.stream.color, 1280, 720, rs.format.bgr8, 30)Inside the main loop we will get color data from the camera and convert it into a NumPy array:
frames = pipeline.wait_for_frames()
color_frame = frames.get_color_frame()
color_image = np.asanyarray(color_frame.get_data())Next we can perform inference using our TensorFlow session:
(boxes, scores, classes, num) = sess.run([detection_boxes, detection_scores, detection_classes, num_detections],
feed_dict={image_tensor: image_expanded})Finally, we will assign random persistent color to each detection class and draw a bounding box around the object. We filter out low confidence predictions using score output.
for idx in range(int(num)):
class_ = classes[idx]
score = scores[idx]
box = boxes[idx]
if class_ not in colors_hash:
colors_hash[class_] = tuple(np.random.choice(range(256), size=3))
if score > 0.8:
left = box[1] * W
top = box[0] * H
right = box[3] * W
bottom = box[2] * H
width = right - left
height = bottom - top
bbox = (int(left), int(top), int(width), int(height))
p1 = (int(bbox[0]), int(bbox[1]))
p2 = (int(bbox[0] + bbox[2]), int(bbox[1] + bbox[3]))
# draw box
r, g, b = colors_hash[class_]
cv2.rectangle(color_image, p1, p2, (int(r), int(g), int(b)), 2, 1)Expected output:

Example 1 : Showing expected output with bounding boxes around objects in the scene.
Part 2 - Augmenting output using Depth data
Since RealSense Cameras also offer per-pixel depth information, we can use this extra data to solve additional problems related to our detection and classification example. In Example 2 we'll use color data to detect people and depth data to quickly estimate the height of each person.
In this example we will configure depth stream in addition to color:
config.enable_stream(rs.stream.depth, 848, 480, rs.format.z16, 30)We'll also need pointcloud and align helper objects for depth data manipulation:
aligned_stream = rs.align(rs.stream.color) # alignment between color and depth
point_cloud = rs.pointcloud()Inside the main loop we will first make sure depth data is aligned to color sensor viewport and next generate an array of XYZ coordinates instead of raw depth:
frames = aligned_stream.process(frames)
depth_frame = frames.get_depth_frame()
points = point_cloud.calculate(depth_frame)
verts = np.asanyarray(points.get_vertices()).view(np.float32).reshape(-1, W, 3) # xyzThis allows us to query XYZ coordinates of each detected object and to separate individual coordinates (in meters):
obj_points = verts[int(bbox[1]):int(bbox[1] + bbox[3]), int(bbox[0]):int(bbox[0] + bbox[2])].reshape(-1, 3)
zs = obj_points[:, 2]
ys = obj_points[:, 1]To avoid outliers we will delete any Y values corresponding to Z values far away from Z median. This makes sure the background has minimal interference with our calculation.
z = np.median(zs)
ys = np.delete(ys, np.where((zs < z - 1) | (zs > z + 1)))Assuming camera is horizontal, persons height can be approximated by its length in Y direction. This can be easily calculated using max and min Y:
my = np.amin(ys, initial=1)
My = np.amax(ys, initial=-1)
height = (My - my)Expected output:

Example 2: Image of a small child with a bounding box showing approximated height.
Part 3 - Deploying TensorFlow model using OpenCV
While TensorFlow is convenient to install and use, it is not as convenient as OpenCV. OpenCV is ported to most platforms and is well optimised for various types of CPUs. It also comes with built-in DNN module capable of loading and using TensorFlow models without having TensorFlow (or its dependencies) installed.
Example 3 is functionally equal to Example 2, but instead of using TensorFlow APIs directly it is loading and running inference using OpenCV.
In addition to the model file, you will need pbtxt file accompanying the model. This file can be found at this link.
net = cv2.dnn.readNetFromTensorflow(r"frozen_inference_graph.pb",
r"faster_rcnn_inception_v2_coco_2018_01_28.pbtxt")After converting color image to NumPy array, inference can be done as follows:
scaled_size = (int(W), int(H))
net.setInput(cv2.dnn.blobFromImage(color_image, size=scaled_size, swapRB=True, crop=False))
detections = net.forward()Resulting detections array will capture all detections and associated information.
Tools
There are several helper tools located under tools folder:
RMSE
RMSE tool can be used to show the surface smoothness by plane-fit RMS of pixels inside a selected rectangle inside the image. The tool is approximating best fit plane passing through selected points, ignoring zero depth and calculates how far on average points are from that plane. When evaluated on planar surface, this gives good metric for surface smoothness. In addition, noise distribution within the selected bounding box is color coded: Black pixels correspond to low deviation from predicted plane-fit with white pixels corresponding to points further always from the plane, normalized by standard deviation.

The RMSE tool.
Convert to Bag
This tool runs on a folder that contains:
1. depth images as captured by D400 series camera
2. ground truth of depth images from #1
3. IR images from left sensor corresponding to #1 and #2
4. denoised images : Unet network model prediction of noisy images from #1The output is a BAG file that could be opened by the RealSense viewer.
Conclusions
This article is showing small number of examples for using deep learning together with RealSense hardware. It is intended to be further extended and you are welcomed to propose enhancements and new code samples. You are also free to use the provided sample code, dataset and model for research or commercial use, in compliance with the RealSense SDK 2.0 License
Updated about 2 months ago