Troubleshooting Tips and Tricks
The following commands can be used to isolate and analyze issues:
Kernel Version
To Retrieve the Kernel Version use:
$ uname -rEnable LibRealSense Log
To change the log level of LibRealSense logger, you need to set a local variable named LRS_LOG_LEVEL and initialize it with the desirable log level:
On Linux:
$ export LRS_LOG_LEVEL="<Log Level>"On Windows:
$ set LRS_LOG_LEVEL="<Log Level>"A LibRealSense log will be created even when an application does not activate the LibRealSense logger.
Connected Intel Cameras
To list all connected Intel Cameras:
$ lsusb | grep 8086General Linux Kernel Log
To retrieve the last Linux Kernel log messages with timestamps:
$ dmesg -TTo clear the dmesg buffer:
$ sudo dmesg -cLinux writes all OS logs to /var/log folder.
To review the entire kernel log file, use:
$ less /var/log/kern.logUVC Video Module Traces
You can get more verbose logs from the uvcvideo kernel-module.
These logs can be seen in dmesg
To enable the UVC driver verbose log:
$ sudo echo 0xFFFF > /sys/module/uvcvideo/parameters/traceTo disable the UVC verbose log, replace 0xFFFF with 0.
For example, once enabled you will get the following line inside dmesg for each frame received from USB:
[619003.810541] uvcvideo: frame 1 stats: 0/0/1 packets, 0/0/1 pts (!early initial), 0/1 scr, last pts/stc/sof 25177741/25178007/81
[619003.810546] uvcvideo: Frame complete (FID bit toggled).
[619003.810556] uvcvideo: frame 2 stats: 0/0/1 packets, 0/0/1 pts (!early initial), 0/1 scr, last pts/stc/sof 25210903/25211168/346
[619003.810588] uvcvideo: uvc_v4l2_poll
[619003.811173] uvcvideo: uvc_v4l2_poll
[619003.843768] uvcvideo: frame 3 stats: 0/0/1 packets, 0/0/1 pts (!early initial), 0/1 scr, last pts/stc/sof 25210903/25211168/346
[619003.843774] uvcvideo: Frame complete (FID bit toggled).
[619003.843785] uvcvideo: frame 4 stats: 0/0/1 packets, 0/0/1 pts (!early initial), 0/1 scr, last pts/stc/sof 25244064/25244330/612Kernel Events
To listen to camera connect/disconnect events:
$ sudo udevadm monitorSystem Calls and Signals
To get a verbose log of all calls an application makes to the kernel, run the application under strace:
$ strace <Application Path>Core Dump File
In case of a crash (for example SEGFAULT), a snapshot of the crash can be created (Core Dump) and submitted for inspection.
- Enable the auto-creation of Core Dump files:
$ ulimit -c unlimited-
Run the application that causes the crash
-
Search for the
corefile in the current directory
NoteAuto-creation of the dump file will only work on the same Terminal that you ran the ulimit command.
Updated 2 months ago