C# (.NET)

These examples demonstrate how to use the .NET wrapper with the RealSense SDK.
They demonstrate how to easily use the SDK to include code snippets that access the camera into your applications.

RealSense SDK 2.0 Installation Guidelines

Installation guidelines with CMake and Visual Studio, Core CLI and Mono are on GitHub

List of RealSense SDK 2.0 Examples

Hello World

Here is a minimal depth application written in C#:

var pipe = new Pipeline();
pipe.Start();

while (true)
{
    using (var frames = pipe.WaitForFrames())
    using (var depth = frames.DepthFrame)
    {
        Console.WriteLine("The camera is pointing at an object " +
            depth.GetDistance(depth.Width / 2, depth.Height / 2) + " meters awayt");

        Console.SetCursorPosition(0, 0);
    }
}

📘 Note:

Since the SDK is holding-on to native hardware resources, it is critical to make sure you deterministically dispose of objects, especially those derived from Frame. Without releasing resources explicitly the Garbage Collector will not keep-up with new frames being allocated.

Example Description Link to GitHub
Depth Streams depth frames for a headless device cs-tutorial-depth
Capture Captures depth and color and renders to side-by-side windows cs-tutorial-capture
Processing Aligns depth to color and applies the post processing filters cs-tutorial-processing
Software development Demonstrates usage of the software_device object, which allows users to create and control custom SDK device cs-tutorial-software-dev
Pose Demonstrates how to obtain data from pose frames cs-tutorial-pose

Last Updated: February 2, 2026

Top
Contact Sales
Server Region: Unknown | Hostname: ip-172-16-1-244 | Visitor Country: Unknown