rs-hello-realsense
Demonstrates the basics of connecting to a RealSense device and using depth data
Overview
rs-hello-realsense example demonstrates the basics of connecting to a RealSense device and taking advantage of depth data by printing the distance to object in the center of camera field of view.
Expected output
Assuming camera is connected you should see "The camera is facing an object X meters away" line being continuously updated. X is the distance in meters to the object in the center of camera field of view.
Code walk-through
First, we include the RealSense Cross-Platform API.
All but advanced functionality is provided through a single header:
#include <librealsense2/rs.hpp> // Include RealSense Cross Platform APINext, we create and start RealSense pipeline. Pipeline is the primary high level primitive controlling camera enumeration and streaming.
// Create a Pipeline - this serves as a top-level API for streaming and processing frames
rs2::pipeline p;
// Configure and start the pipeline
p.start();Once pipeline is configured, we can loop waiting for new frames.
RealSense cameras usually offer multiple video, motion or pose streams.
wait_for_frames function will block until next set of coherent frames from various configured streams.
// Block program until frames arrive
rs2::frameset frames = p.wait_for_frames();To get first frame from the depth data stream, you can use get_depth_frame helper function:
// Try to get a frame of a depth image
rs2::depth_frame depth = frames.get_depth_frame();Next we query the default depth frame dimensions (these may differ from sensor to sensor):
// Get the depth frame's dimensions
float width = depth.get_width();
float height = depth.get_height();To get distance at specific pixel (center of the frame), you can use get_distance function:
// Query the distance from the camera to the object in the center of the image
float dist_to_center = depth.get_distance(width / 2, height / 2);The only thing left is to print the resulting distance to the screen:
// Print the distance
std::cout << "The camera is facing an object " << dist_to_center << " meters away \r";That's it!
Updated about 2 months ago