rs-sensor-control
A tutorial for using the rs2::sensor API
Overview
The sensor control samples aims to provide the entry point and a tutorial for using the more advanced API that the RealSense SDK provides.
In addition to the r2::pipeline API, which simplifies streaming flow, the SDK provides the rs2::context, rs2::device, and rs2::sensor APIs that provide an abstraction for RealSense devices.
In this sample we show how to use this API for querying all connected devices, their sensors, and their streams.
Using a rs2::sensor one can control a camera's options, stream from it, and get the frames directly without having them processed or synchronized (as the rs2::pipeline does).
Expected Output
Running this example with a connected RealSense device, will output the connected device names, and requests the user to select a camera (or connect one).
After selecting a camera, the user will be prompt to select one of the device's sensor, and select which action to perform using that sensor.
This flow will repeat itself as long as the user desires.
Code Overview
Please follow the api_how_to.h for detailed documentation and explanations
This file contains detailed explanations and code on how to do the following:
Updated 2 months ago